To compare local projects, use the Compare Projects function from the File menu.
The Compare PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Programs tool is accessed from a button on the Status Bar, between the Local and Controller versions. It is active when KAS is connected to a controller.
Figure 4-71: Difference in Local and Controller Versions
Click the button to open the list of items for both versions. Red item indicates where there is a mismatch. Double-click to open an item. The << button brings you back to the list.
Figure 4-72: Listing the Differences
The following message will be shown if you click on the compare button but the project is not present on the controller.
Limitation with FFLD Diagrams
If one or more components within a network differ, then the entire network is displayed in the diff view with a gray background. Differences between individual components within the network are not specified in any way.
For example, in the following image we have a comparison of two FFLD programs.
|
Copyright © 2015 Kollmorgen™ |
|